Note: This feature is available only for power meters and power sensors that support trace charts shown in the Trace display view.
The Power Meter application allows you to determine various measurements within a trace graph. Captured trace data can be displayed in a trace graph for you to determine parameter values and perform simple measurement analyses. You can acquire parameter values of the graph according to a set of predefined parameters. In addition, you can determine the range of the graph for parameter value acquisition using the GateA set of vertical limit lines drawn on the graph to mark the boundaries of specific areas of interest. or MarkerA vertical or horizontal indicator placed on the graph to act as a pointer. function.